Flowmeter verification with Heartbeat Technology
Maximise your plant availability and optimize your maintenance cost
The manufacturing industry has long been essential to Indonesia's economic growth. The government of Indonesia even planned to make the country one of the ten countries with the highest economic power. Knowing that industrial processes are critical key factors in the manufacturing industry, Endress+Hauser come up with products, solutions and services to help industries optimally run their processes. One of which is flowmeter verification with Heartbeat Technology.
Benefits
Diagnostic.
Refers to the ability to perform reliable self-monitoring with easy-to-understand diagnostic messages that the plant operator can easily identify once errors arise.This function can prevent unnecessary downtime or decreased production due to undetected issues.
Diagnostic messages may appear in five status signals: diagnostic active, failure, function check, out of specification and maintenance required. Each status signal indicates a specific condition needing a particular action to resolve.
Verification.
The verification function not only checks that the device components are still within predefined limits, but also indicates any errors that may cause a problem with the device's performance.As Heartbeat verification is a traceable verification method according to ISO 9001, it can be used to extend calibration intervals.
The plant operator may print the documented proof of a performed verification. The corresponding Heartbeat Technology verification report can be used as a quality document documenting the current device state.
Monitoring.
This function enables predictive maintenance by identifying process conditions that may affect device or asset integrity or process performance, e.g., the occurrence of foam in a tank, corrosion, or build-up on the sensor surface.The response from the sensor is converted to easy-to-understand information, assisting the plant operator to foresee and plan any maintenance activities accordingly.
Taking the pulse of your instruments
Despite the essential role of the manufacturing industry in Indonesia’s economic growth and the interest of many foreign investors in this sector, business owners are still facing one major challenge, which is production costs. Affected by many variables such as labour, logistics, and maintenance costs, it can force companies to increase the sales price to cover production costs or may result in a decline in sales or loss of customers.
Flowmeter verification with Heartbeat Technology can help companies combat such issues. Its ability to do continuous self-diagnostics without removing the device or stopping production enables significant production improvement. In addition, this technology can also identify specific device problems so that dedicated corrective actions can be taken.
Its capability to support the operator to predict maintenance requirements also brings clear efficiency gains, as well as reducing the risk of undesired product quality or product loss. Heartbeat Technology's functions help manufacturing companies avoid unnecessary production costs. e.g., repeated downtime due to undetected issues on critical instruments, unnecessary frequent calibration, or manually performing device functionality assessments.

Downloads
-
Heartbeat Technology Brochure.pdf
File size:
9.2 MB
File name:
Heartbeat Technology Brochure.pdf